Hi,
In the sample project Wireless Uart, there is a section of code in wireless_uart.c like this:
//-------------------------
void BleApp_StateMachineHandler(deviceId_t peerDeviceId, uint8_t event)
{
uint16_t tempMtu = 0;
/* invalid client information */
if(gInvalidDeviceId_c == maPeerInformation[peerDeviceId].deviceId)
{
return;
}
switch (maPeerInformation[peerDeviceId].appState)
{
case mAppIdle_c:
{
if (event == mAppEvt_PeerConnected_c)
{
/* Let the central device initiate the Exchange MTU procedure*/
if (mGapRole == gGapCentral_c)
{
/* Moving to Exchange MTU State */
maPeerInformation[peerDeviceId].appState = mAppExchangeMtu_c;
GattClient_ExchangeMtu(peerDeviceId);
}
else
{
/* Moving to Service Discovery State*/
maPeerInformation[peerDeviceId].appState = mAppServiceDisc_c;
/* Start Service Discovery*/
BleServDisc_FindService(peerDeviceId,
gBleUuidType128_c,
(bleUuid_t*) &uuid_service_wireless_uart);
}
}
}
break;
//-------------------
It shows if the device is a Peripheral device, BleServDisc_FindService needs to be called. But from my point of view, BleServDisc_FindService is a API for Central device, not for Peripheral.
So, why BleServDisc_FindService needs to be called here ?
B.R
Daniel Xiao