CLRC663 + NxpNfcRdLib FCC Testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 + NxpNfcRdLib FCC Testing

1,795件の閲覧回数
mraines
Contributor I

Are there instructions or examples for placing the CLRC663 in CW transmit mode for FCC testing? I found phhalHw_Rc663_Cmd_PRBS() but also discovered other pre-configurations are necessary. For example, the waterlevel register must be explicitly configured and the field must be manually switched on.

Is anything else necessary or recommended?

0 件の賞賛
返信
1 返信

1,770件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @mraines ,

 

There is no ready example for CLRC663 regarding FCC testing, but there is an example based on PN7150 for this topic, you may use it as a reference. Please kindly refer to https://github.com/NXP/nfc-linux_NfcFactoryTestApp for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信