Bootloader in KW45

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,957件の閲覧回数
Chan_17
Contributor III

Can we build custom bootloader for KW45 ? 

Can we program other MCU using KW45 (consider other MCU can be reprogrammed via  its spi) , so here how can we give other MCU hexfile/firmware to KW45 . Please let us know if there is any Application note

0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello,

The NTM88 is an old sensor; I would recommend redirect this question to Analog and Sensors Community to find more information regarding the NTM88.

Here is a Link for it Sensors - NXP Community

I really apologize for the inconveniences this might cause you and your project.

What you could review is this Application note that describes using NTM88 with a MCU Host, please check this guide to see if adjust to your necessities.

Implementing Wired Communication with the NTM88  AN14182, Implementing Wired Communication with the NTM88 - Application Note

Thank you for your interest in NXP Semiconductor products

Best Regards

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,894件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello,

 

Could you help us explain more details about what you trying to achieve?

Are you using a KW45 EVK board? Or the KW45 in a custom board?

Could this Application note available for KW45 explain what you trying to achieve? Please refer to introduction section.

Custom Bootloader using OTAP--AN13860

Creating Firmware Update Image for KW45B41Z/K32W148 using Over the Air Programming Tool

Custom Bootloader with Fuses--AN13883

Updating KW45 Radio Firmware Via ISP Using SPSDK

 

Best Regards

Luis

0 件の賞賛
返信
1,841件の閲覧回数
Chan_17
Contributor III

hI Luis,

Thanks for replying!

We are using KW45 EVK board . We want to program NTM88 MCU via spi of other MCU (this application note is there in NTM88 documentation https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/sensors/8058/1/NTM88_SPI_Reprogramming_r...). In our case other MCU is KW45 . So to program NTM88 through KW45 we need to take firmware of NTM88 inside kw45 first and then with spi we need to transfer it to NTM88 .   This is what we want to achieve . Is it possible then how?

0 件の賞賛
返信
1,822件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello,

The NTM88 is an old sensor; I would recommend redirect this question to Analog and Sensors Community to find more information regarding the NTM88.

Here is a Link for it Sensors - NXP Community

I really apologize for the inconveniences this might cause you and your project.

What you could review is this Application note that describes using NTM88 with a MCU Host, please check this guide to see if adjust to your necessities.

Implementing Wired Communication with the NTM88  AN14182, Implementing Wired Communication with the NTM88 - Application Note

Thank you for your interest in NXP Semiconductor products

Best Regards

Luis

0 件の賞賛
返信
1,913件の閲覧回数
Chan_17
Contributor III

Please check , we struck in this .

0 件の賞賛
返信