Bluetooth connection issue in imxul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bluetooth connection issue in imxul

1,440 次查看
bulkesh
Contributor I

Hi We are working on imx6ul. There is an issue with bluetooth connection , as we are able to pair, scan but not able to connect with bluetooth devices

below are the logs

root@imx6ulevk:~# bluetoothctl
Agent registered
[bluetooth]# scan on
Discovery started
[CHG] Controller D4:53:83:05:49:D5 Discovering: yes
[NEW] Device 70:BB:E9:4C:C5:79 Redmib
[NEW] Device 70:1C:E7:96:52:11 90100--IOT--GGN
[bluetooth]# scan off
Discovery stopped
[CHG] Controller D4:53:83:05:49:D5 Discovering: no
[CHG] Device 70:1C:E7:96:52:11 TxPower is nil
[CHG] Device 70:1C:E7:96:52:11 RSSI is nil
[CHG] Device 70:BB:E9:4C:C5:79 RSSI is nil
[bluetooth]# pair 70:BB:E9:4C:C5:79
Attempting to pair with 70:BB:E9:4C:C5:79
[CHG] Device 70:BB:E9:4C:C5:79 Connected: yes
Request PIN code
[agent] Enter PIN code: 1234
[CHG] Device 70:BB:E9:4C:C5:79 Modalias: bluetooth:v000Fp1200d1436
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001105-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110a-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110c-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000110e-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001112-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001115-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001116-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000111f-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112d-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 0000112f-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001132-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001200-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001800-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 00001801-0000-1000-8000-00805f9b34fb
[CHG] Device 70:BB:E9:4C:C5:79 UUIDs: 98b97136-36a2-11ea-8467-484d7e99a198
[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: yes
[CHG] Device 70:BB:E9:4C:C5:79 Paired: yes
Pairing successful
[CHG] Device 70:BB:E9:4C:C5:79 ServicesResolved: no
[CHG] Device 70:BB:E9:4C:C5:79 Connected: no
[bluetooth]# connect 70:BB:E9:4C:C5:79
Attempting to connect to 70:BB:E9:4C:C5:79
Failed to connect: org.bluez.Error.Failed
[bluetooth]#

Kindly help

0 项奖励
回复
1 回复

1,410 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

hello,

 

Could you please help me with the Bluetooth part you are using ?

 

Regards,

Estephania

0 项奖励
回复