Block data is not read correctly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Block data is not read correctly

1,910 Views
eric_wanghao
Contributor I

Hello,

I have a question about RC663 when reading  an ISO15693 card.The source program is shown in the attachment.   

Block data  returned is always 0x5a 0xf 0x0 0x20,whatever the block number is.I've been puzzled by this problem for a long time.Please read the source code in the attachment carefully and try to find out the corresponding reasons.

p.s.I use the NxpNfcRdLib to program.

Thanks a lot!

0 Kudos
Reply
1 Reply

1,756 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hope you are doing great, can you tell me which example are you using or if you are modifying an example in the library if that is the case which example you are using as base to your project.

I am checking with the 15693 example and it works fine. also which library version do you have.

Have a great day !

BR

Jonathan

0 Kudos
Reply