Beyondstudio with sharedrive (network)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Beyondstudio with sharedrive (network)

3,108件の閲覧回数
zigbee1
Contributor III

I'm having a problem to get a setup with some of the SDK and the workspace on a remote drive.

Here is a screenshoot of the Build errors. It looks like the z: drive is not recognized

I have also use mklink /d to create symbolic links but this doesn't help !

Any suggestions, recommendation on how/what to do ?

1 返信

3,079件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Patrick, I hope you're doing well!

 

We recommend using the default path of installation for the BeyondStudio IDE, as changing it can cause issues like the ones you're experiencing.

 

Could you please take a look at the following document for information about BeyondStudio Common Errors?

 

Please let me know if you need any more information.

 

Best regards,

Sebastian