BeyondStudio C files open just like text.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BeyondStudio C files open just like text.

1,411件の閲覧回数
LChll
Contributor III

Under Win10, BeyondStudio installed, after importing JA-AN-1220 project, some files showed abnormal.I can't even navigate the code smoothly.

Engineering compilation is ok.Why is this happening?

C files open just like text.

The same goes for reinstalling BeyondStudio, and the project is the latest download.

normal.pngis not normal.png

ad
0 件の賞賛
返信
1 返信

1,402件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @LChll,

I am not sure if you have some issues in your installation process.

However, if you are seeing the file as a text editor, you could select the c editor.

mario_castaneda_0-1607712532324.png

 

Also, please look at the next community post if you have any further issues with Beyond Studio.

Let me know if you have any further issue.

Regards,

Mario

 

0 件の賞賛
返信