BLE sample application is not working on FRDM-MCXW71

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE sample application is not working on FRDM-MCXW71

1,202 Views
Rathore-pioneer
Contributor III

Please help me to setting up BLE as peripheral role for MCXW71 EVK.

I already try some sample applications for led control and hello world application which are working fine.

But available BLE sample are not working.

List of BLE sample application which I tried:

  1. frdmmcxw71_eatt_peripheral_freertos
  2. frdmmcxw71_eatt_peripheral_bm
  3. frdmmcxw71_ble_shell_freertos

 

while debugging the sample app it’s getting stuck in APP_InitBle() à  PLATFORM_SetBleMaxTxPower() à Controller_SetMaxTxPower() function.

it’s coming into assert condition:

Rathorepioneer_0-1745243430936.png

 

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,151 Views
sofiaurueta
NXP Employee
NXP Employee

Hope you’re doing well.

 

Could you please help me confirm your SDK version and if you installed the NBU firmware for MCXW71?

 

It is necessary to work with the matching NBU image for the SDK version of the application you are working with. This means that when you download your SDK, prior to loading any wireless SDK example, update your NBU image with the provided binaries in the SDK folder.

 

If you could follow this guide: Getting Started with FRDM-MCXW71 section 3.

 

Best Regards,

Ana Sofia.

0 Kudos
Reply