BLE "Programmable transmit output power"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE "Programmable transmit output power"

1,898件の閲覧回数
valentinberthom
Contributor I

Hello,

On the datasheet, of the KW3xx KW4xx chips, its stated that  BLE has a "Programmable transmit output power from -18 dBm to +5 dBm with DC/DC bypass and buck modes of operation" I would like to know what precision I could get in term of transmit power configuration?

Thank you,

Valentin

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,608件の閲覧回数
antonioconcio
NXP Employee
NXP Employee

Hi Valentin,

Please refer to the file "BLEADG.pdf" at the following path: C:\Freescale\KW40Z_Connectivity_Software_1.0.1\ConnSw\doc

pastedImage_1.png

Hope this helps,

Antonio

0 件の賞賛
返信

1,608件の閲覧回数
sensenthuran
Contributor IV

If we are using the hci_app.bin for kw40/41z, how we can change the tx  power dynamically with bluez antonioconcio

The default value is set:

/app/common/ble_controller_task_config.h

#ifndef mAdvertisingDefaultTxPower_c

#define mAdvertisingDefaultTxPower_c    0

#endif

0 件の賞賛
返信