BLE Carrier Wave and Modulation options

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BLE Carrier Wave and Modulation options

跳至解决方案
3,003 次查看
alexishernandez
Contributor III

Hi community, i'm using the MKW40 BLE Module and i want to know if there is any way to enable/disable the modulation, enable/disable the radio and the carrier wave without modulation.

From the KW40Zxx Reference Manual :

Chapter 44: Use of the radio will be facilitated through firmware provided by Freescale giving
customers access to all the radio features through appropriate API interfaces. As such,
detailed information on radio control registers is not provided here.
Where are those appropriate API interfaces?
Best regards.

标签 (3)
1 解答
2,614 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,615 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alexis Hernandez

Please check the followings community posts:

NXP connectivity FCC/ETSI Certification Software 

https://community.nxp.com/docs/DOC-332721 

There is already examples codes that allows you to test radio in the connectivity software, I recommend you to check them, also please check the code to find out how radio is set.

Hope this information could help you, please let me know if you have any question about this.

Best Regards

Jorge Alcala

0 项奖励
回复