BGU7045 - switch time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BGU7045 - switch time

666件の閲覧回数
ricardopereira
Contributor I

Hi, 

There is no information on the datasheet about how fast does the BGU7045 switch between 14dB Gain mode to Bypass mode. Can you provide it please? 

Thank you for your time,

0 件の賞賛
返信
1 返信

583件の閲覧回数
LPP
NXP Employee
NXP Employee

NXP does not specify switch time but our RF application engineer measured it as following:

By using 3V at control line (pin 4) then the on time is 12us and the off (bypass) time is 19us .
Lowering the control voltage will lead to increase the switch time!


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信