BGU7045 - switch time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BGU7045 - switch time

665 Views
ricardopereira
Contributor I

Hi, 

There is no information on the datasheet about how fast does the BGU7045 switch between 14dB Gain mode to Bypass mode. Can you provide it please? 

Thank you for your time,

0 Kudos
Reply
1 Reply

582 Views
LPP
NXP Employee
NXP Employee

NXP does not specify switch time but our RF application engineer measured it as following:

By using 3V at control line (pin 4) then the on time is 12us and the off (bypass) time is 19us .
Lowering the control voltage will lead to increase the switch time!


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply