Arrays and Structures support in ZCL (ZigBee)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Arrays and Structures support in ZCL (ZigBee)

1,505 次查看
bogdan_kostiv
Contributor I

Hi,

I'm working on a ZigBee solution where custom clusters will be used. In some clusters I would like to use arrays (E_ZCL_ARRAY = 0x48) and structures (E_ZCL_STRUCT = 0x4c). But as I see proper implementation of mentioned data types is missing. I'm wondering if there are plans to add support of arrays and structures to the ZCL.

BR,

Bogdan

0 项奖励
回复
1 回复

1,418 次查看
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Bodgan,

Unfortunately, right now, we do not have any implementation with the array or struct to the ZCL. We are working on a maintenance release for the Zigbee Stack. It is a good implementation but we do not have any plans for supporting this feature.

Regards,

Mario

0 项奖励
回复