Application node files won't open in beyond studio for NXP (JN_AN_1218)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application node files won't open in beyond studio for NXP (JN_AN_1218)

2,336件の閲覧回数
dirk_van_grunsv
Contributor II

Hi!

I have some trouble with the JN-AN-1218. this application node won't open in beyond studio for NXP. I have followed the steps from JN-UG-3101 and I see the project in the project explorer, but the resource does not exist.

product: JN5168-001-M00

IDE: Beyond studio for NXP JN-SW-4141

installed SDK : JN-SW-4170

problematic application node: JN-AN-1218

0 件の賞賛
返信
3 返答(返信)

2,251件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dirk,

Did you save the example in the BeyondStudio installation directory under C:\NXP\bstudio_nxp?

Could you please provide a screen of the issue that you are facing?

Regards,

Mario

0 件の賞賛
返信

2,251件の閲覧回数
dirk_van_grunsv
Contributor II

I saved the Aplication Node in C:\NXP\bstudio_nxp\workspafe following the BeyondStudio for NXP installation and User Guide (JN-UG-3098)

first I imported the project(JN-AN-1218)

pastedImage_1.png

than it should be visable in the project explorer

pastedImage_3.png

I get all these yellow ! and I can't open the files. I followed the same path with the JN-AN-1171 and this works just fine.

Do you know what may be cousing the problem? I installed the right SDK for ZigBee 3.0 (JN-SW-4170) before this process.

0 件の賞賛
返信

2,251件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Dirk,

Please look at the https://community.nxp.com/docs/DOC-340028 

You should not select the option JN517X, it is not supported by Beyond Studio IDE

Regards,

Mario

0 件の賞賛
返信