Advertising / Scanning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Advertising / Scanning

2,166件の閲覧回数
alejandropérez
Contributor II

On the one hand, I have a KW41Z sending advertising packets during 4 seconds. On the other hand, I have a KW41Z scanning during 20ms every 2s.

The problem is that I don't have guarantee of the correctly reception of the information. For this reason, I need to confirm that the information is receceived, otherwise send again the advertising packet. How can I do this?

Thanks in advance.

ラベル(2)
0 件の賞賛
返信
1 返信

1,987件の閲覧回数
gerardo_rodriguez
NXP Employee
NXP Employee

Hello Alejandro Pérez,

Can you share the advertising parameters (gAdvParams) and scanning parameters (gScanParams) that you are using?

You may need to increase the advertising interval or the scanning window to ensure that the advertisement packets have enough time to be received.

0 件の賞賛
返信