Adding Secure Coap support in K32W(openthread stack)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Adding Secure Coap support in K32W(openthread stack)

3,016 次查看
sd05
Contributor III

I am trying to compile the reed example with minimal secure coap code but in the process i am getting following error for mbedtls
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: /home/sunidhi/Downloads/bae/openthread/ot-nxp/build_k32w061/lib/libmbedtls.a(ssl_tls.c.obj): in function `mbedtls_ssl_config_defaults':
ssl_tls.c:(.text.mbedtls_ssl_config_defaults+0xa8): undefined reference to `mbedtls_x509_crt_profile_suiteb'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: ssl_tls.c:(.text.mbedtls_ssl_config_defaults+0xb4): undefined reference to `mbedtls_x509_crt_profile_default'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: /home/sunidhi/Downloads/bae/openthread/ot-nxp/build_k32w061/lib/libmbedtls.a(ssl_tls.c.obj): in function `mbedtls_ssl_parse_certificate':
ssl_tls.c:(.text.mbedtls_ssl_parse_certificate+0xda): undefined reference to `mbedtls_x509_crt_init'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: ssl_tls.c:(.text.mbedtls_ssl_parse_certificate+0xf2): undefined reference to `mbedtls_x509_crt_free'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: ssl_tls.c:(.text.mbedtls_ssl_parse_certificate+0x186): undefined reference to `mbedtls_x509_crt_verify_restartable'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: ssl_tls.c:(.text.mbedtls_ssl_parse_certificate+0x1d2): undefined reference to `mbedtls_x509_crt_free'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: ssl_tls.c:(.text.mbedtls_ssl_parse_certificate+0x26e): undefined reference to `mbedtls_x509_crt_parse_der_nocopy'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: /home/sunidhi/Downloads/bae/openthread/ot-nxp/build_k32w061/lib/libopenthread-ftd.a(dtls.cpp.obj): in function `ot::MeshCoP::Dtls::FreeMbedtls()':
dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls11FreeMbedtlsEv+0x10): undefined reference to `mbedtls_x509_crt_free'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls11FreeMbedtlsEv+0x18): undefined reference to `mbedtls_x509_crt_free'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: /home/sunidhi/Downloads/bae/openthread/ot-nxp/build_k32w061/lib/libopenthread-ftd.a(dtls.cpp.obj): in function `ot::MeshCoP::Dtls::SetApplicationCoapSecureKeys()':
dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls28SetApplicationCoapSecureKeysEv+0x22): undefined reference to `mbedtls_x509_crt_parse'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls28SetApplicationCoapSecureKeysEv+0x44): undefined reference to `mbedtls_x509_crt_parse'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: /home/sunidhi/Downloads/bae/openthread/ot-nxp/build_k32w061/lib/libopenthread-ftd.a(dtls.cpp.obj): in function `ot::MeshCoP::Dtls::Setup(bool)':
dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls5SetupEb+0x30): undefined reference to `mbedtls_x509_crt_init'
/usr/local/mcuxpressoide-11.4.1_6260/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.4.0.202103011116/tools/bin/../lib/gcc/arm-none-eabi/10.2.1/../../../../arm-none-eabi/bin/ld: dtls.cpp:(.text._ZN2ot7MeshCoP4Dtls5SetupEb+0x38): undefined reference to `mbedtls_x509_crt_init'

0 项奖励
回复
3 回复数

2,996 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Could you please describe the procedure you followed?

Can you clarify what do you mean with "reed example with minimal secure coap code"?

 

Best Regards,

Ricardo

0 项奖励
回复

2,981 次查看
sd05
Contributor III

Hello @Ricardo_Zamora 

I am developing an apps based on k32w061dk6_reed_ble_wuart_bm example where i need to add the secure coap support. I added following lines in  <Proj Dir>/MCUXpresso_11.4.1_6260/workspace/k32w061dk6_reed_ble_wuart_bm/source/reed_app.c

otCoapSecureSetSslAuthMode(gpOpenThreadInstance, false);
otCoapSecureSetClientConnectedCallback(gpOpenThreadInstance, HandleConnected, NULL);

otCoapSecureSetDefaultHandler(gpOpenThreadInstance, DefaultHandler, NULL);


otCoapSecureStart(gpOpenThreadInstance, OT_DEFAULT_COAP_SECURE_PORT);

I tried defining OPENTHREAD_CONFIG_COAP_SECURE_API_ENABLE as 1 in <Proj Dir>/MCUXpresso_11.4.1_6260/workspace/k32w061dk6_reed_ble_wuart_bm/source/config.h

and when I tried to build I am getting following errors

undefined reference to `otCoapSecureSetClientConnectedCallback'

undefined reference to `otCoapSecureSetDefaultHandler'

undefined reference to `otCoapSecureStart'

Please guide the steps to enable the secure coap support in K32W SDK 2_6_4.

Thanks!!

0 项奖励
回复

2,977 次查看
sd05
Contributor III

Also one more question what are the steps to make changes in openthread libraries available with the SDK

0 项奖励
回复