Add a zone to IAS device command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add a zone to IAS device command

1,487 Views
rostislav
Contributor III

I created a IAS ZED using Freescale beekit V 3.0.2 To make it operational I need adding a zone with IASZone_AddEntryInClientTable command (Group 0x70 Opcode 0x7E).

Unfortunatelu I couldn't find such command neither in BlackBox document  BSBBZTCRM Rev. 1.4 10/2013 nor in Command Console command list of Freescale Test tool 12 V 12.4.0.

Does exist an updated document? If it is presented in Freescale Test tool 12 V 12.4.0 then which name is used for the command?

0 Kudos
Reply
0 Replies