About output state in the OFF state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About output state in the OFF state

1,183 次查看
tomo
Contributor II

Hi, all.

As BGU8007, BGU8009 and BGU8103 has ENABLE pin.
ENABLE=Low means OFF state according to the datasheet.
Does output become to Hi-Z when OFF state?

best regards,

tomo

标记 (1)
0 项奖励
回复
1 回复

1,135 次查看
LPP
NXP Employee
NXP Employee

When device is disabled, the internal transistor biasing is turned off and device doesn't consume supply power.

Note. Output is AC coupled. AC impedance is not HiZ when device is disabled.

Have a great day,

Pavel
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复