About output state in the OFF state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About output state in the OFF state

1,161 Views
tomo
Contributor II

Hi, all.

As BGU8007, BGU8009 and BGU8103 has ENABLE pin.
ENABLE=Low means OFF state according to the datasheet.
Does output become to Hi-Z when OFF state?

best regards,

tomo

Tags (1)
0 Kudos
Reply
1 Reply

1,113 Views
LPP
NXP Employee
NXP Employee

When device is disabled, the internal transistor biasing is turned off and device doesn't consume supply power.

Note. Output is AC coupled. AC impedance is not HiZ when device is disabled.

Have a great day,

Pavel
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply