AFT09MS015NT1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFT09MS015NT1

12,475件の閲覧回数
赵壮钦
Contributor III

_0-1676028936788.png

HELLO!

Our company purchased this model AFT09MS015NT1. After testing, we found these two problems. How can we solve them?

Attached is the test report

0 件の賞賛
返信
3 返答(返信)

12,465件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Are you using any of our reference designs? Anyway, please check the Application note: RF LDMOS Optimum Biasing Circuit
https://www.nxp.com/docs/en/application-note/AN1643.pdf

Hope it helps.

0 件の賞賛
返信

12,422件の閲覧回数
赵壮钦
Contributor III

你好!

Thank you very much,We are not using biasing method described in NXP AN1643.pdf. That method is not the optimum for TETRA application (Pout +36dBm, Temperature -20 to +55degC, Vdd 10.8 to 15.6V).

Did you use the 046 in the same application as the 052 ( the part that was working properly)? - Yes both were used in same application and also tried on the same board (replacing one with another and only one of them worked)

0 件の賞賛
返信

12,418件の閲覧回数
赵壮钦
Contributor III

HELLO!

The attached pictures are as follows

0 件の賞賛
返信