AFT09MS015NT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AFT09MS015NT1

12,466 Views
赵壮钦
Contributor III

_0-1676028936788.png

HELLO!

Our company purchased this model AFT09MS015NT1. After testing, we found these two problems. How can we solve them?

Attached is the test report

0 Kudos
Reply
3 Replies

12,456 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Are you using any of our reference designs? Anyway, please check the Application note: RF LDMOS Optimum Biasing Circuit
https://www.nxp.com/docs/en/application-note/AN1643.pdf

Hope it helps.

0 Kudos
Reply

12,413 Views
赵壮钦
Contributor III

你好!

Thank you very much,We are not using biasing method described in NXP AN1643.pdf. That method is not the optimum for TETRA application (Pout +36dBm, Temperature -20 to +55degC, Vdd 10.8 to 15.6V).

Did you use the 046 in the same application as the 052 ( the part that was working properly)? - Yes both were used in same application and also tried on the same board (replacing one with another and only one of them worked)

0 Kudos
Reply

12,409 Views
赵壮钦
Contributor III

HELLO!

The attached pictures are as follows

0 Kudos
Reply