AFM907 ADS Model file missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AFM907 ADS Model file missing

2,019 Views
dlaturell
Contributor III

The FET2 model file is missing from the ADS Design Kit.

Please advise when this error will be fixed.

ADS will not work with NXP AFM907 library.

Labels (1)
0 Kudos
Reply
1 Reply

1,917 Views
LPP
NXP Employee
NXP Employee


Installation of the RF High Power Model Kit is required to run all RF High Power ADS models.
FET2 model is a part of the this kit.

So, you must install two kits: RF High Power Model Kit and AFM907N Model Design Kit. Both are provided on the AFM907 product page:

AFM907N|8 W CW, 136-941 MHz, 7.5 V | NXP 


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply