AFM907 ADS Model file missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFM907 ADS Model file missing

2,040件の閲覧回数
dlaturell
Contributor III

The FET2 model file is missing from the ADS Design Kit.

Please advise when this error will be fixed.

ADS will not work with NXP AFM907 library.

ラベル(1)
0 件の賞賛
返信
1 返信

1,938件の閲覧回数
LPP
NXP Employee
NXP Employee


Installation of the RF High Power Model Kit is required to run all RF High Power ADS models.
FET2 model is a part of the this kit.

So, you must install two kits: RF High Power Model Kit and AFM907N Model Design Kit. Both are provided on the AFM907 product page:

AFM907N|8 W CW, 136-941 MHz, 7.5 V | NXP 


Have a great day,

Pavel
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信