88Q9098 kernel linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,080件の閲覧回数
juliana_rojas30
Contributor III

Hello community!

I am reading about the WiFi module 88Q9098 and I see that it supports Linux, but I can't find which kernel is needed for the implementation. Where can I find this data? Which kernel would we need in order to assemble this module?

Thanks!

0 件の賞賛
返信
1 解決策
3,058件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Juliana, I hope you're doing well!

 

The Linux kernel version supported by the latest driver release for the 88Q9098 are from Kernel version 2.6.32 to 5.8.0.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,058件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Juliana, I hope you're doing well!

 

The Linux kernel version supported by the latest driver release for the 88Q9098 are from Kernel version 2.6.32 to 5.8.0.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

0 件の賞賛
返信