88Q9098 kernel linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

88Q9098 kernel linux

Jump to solution
3,080 Views
juliana_rojas30
Contributor III

Hello community!

I am reading about the WiFi module 88Q9098 and I see that it supports Linux, but I can't find which kernel is needed for the implementation. Where can I find this data? Which kernel would we need in order to assemble this module?

Thanks!

0 Kudos
Reply
1 Solution
3,058 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Juliana, I hope you're doing well!

 

The Linux kernel version supported by the latest driver release for the 88Q9098 are from Kernel version 2.6.32 to 5.8.0.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

View solution in original post

0 Kudos
Reply
1 Reply
3,058 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Juliana, I hope you're doing well!

 

The Linux kernel version supported by the latest driver release for the 88Q9098 are from Kernel version 2.6.32 to 5.8.0.

 

Please let me know if you need any more information.

 

Best regards,

Sebastián

0 Kudos
Reply