10Base-T1S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

10Base-T1S

3,853 Views
Damodara_S
Contributor I

Hello Team,

We are developing a 10Base-T1S product which should support 802.1AS, MACsec features and other PLCA features.

Please suggest us any device available from NXP that supports above features.

Thank you.

Regards,

Damodara

0 Kudos
Reply
3 Replies

1,616 Views
RekhaK16
Contributor I

Hi, are there any NXP microcontrollers that support 10BASE-T1 in the Ethernet controller MAC?

0 Kudos
Reply

3,825 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Damodara,

Currently there is no device available in NXP portfolio supporting such features.

When it comes to the 10BASE-T1S, we have the TJA1410 AFE with communication over the simple 3-pin interface standardized in the Open Alliance TC14.

Please note that the TJA1410 is currently in pre-production status and if you require any technical or commercial information, you must reach out to NXP FAE or Sales.

BRs, Tomas

0 Kudos
Reply

2,816 Views
esion1
Contributor I

 Can I buy TJA1410 AFE chip although it's in pre-production status? We also developing 10base-t1s system with FPGA platform. We need analog transceiver like as TJA1410 AFE.

Tags (1)
0 Kudos
Reply