Dear @kbpanchal005
If I am correct you are currently using PCIE-WLAN-UART-BT-9098-U16-X86-17.68.1.p81-17.26.1.p81-MXM5X17277_V0V1-MGPL.zip software.
These FP68 (17.68.1) software releases are restricted access releases, so requiring NDA and access permission procedures, which can take long.
We now promote generic FP92 software releases, which includes most of the FP68 releases features, and are available to all customers without restriction.
These generic software releases are available on NXP github:
- NXP Wifi/BT driver:
git clone http://github.com/nxp-imx/mwifiex.git
git checkout lf-6.1.55-2.2.0
The driver code supports Linux kernel from 2.6.32 to 6.5.4.
- NXP Wifi/BT firmware:
git clone https://github.com/NXP/imx-firmware
git checkout lf-6.1.55-2.2.0
Corresponding release note is available here: https://www.nxp.com/docs/en/release-note/RN00104.pdf
Do you really want to keep your request for latest FP68 software, or don't you want to use generic FP92 software ?
Regards,
Olivier