MCXW23 Transmitter Maximum Output Power Override Application Note

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCXW23 Transmitter Maximum Output Power Override Application Note

MCXW23 Transmitter Maximum Output Power Override Application Note

1       Introduction

As documented in the MCX W23 [ERRATA] for WLCSP packaged devices, Tx modulation quality can potentially be violated on 2 data channels, i.e. channels 15 (2432 MHz) and 31 (2464 MHz) in the Long Range (coded) PHY modes. All other channels are not affected. Also the non-coded PHY modes (1 Mbps and 2 Mbps) are not affected.

 

The occurrence is low, but highest for high transmit output powers. For this reason, the maximum output power has by default been limited to 2 dBm on these 2 channels.

 

Since the Tx modulation performance testing aims to ensure interoperability between different Bluetooth Low Energy devices and has no impact on regulatory requirements, users could override the default configured limit on maximum output power for these 2 concerned channels. Bluetooth Low Energy (BLE) compliance testing (RFPHY.TS, PFPHY/TRM/BV – 13-C) does not cover these 2 channels.

 

2     Overriding the transmitter output power limit

2.1      API command

 

An API command is available, which allows a user to override the Transmitter output power limit of 2 dBm and configure at a higher level.

API command:

Command

OCF

Command arguments

Return parameters

HCI_CMD_OCF_LIMIT_PHY _TX

0x0338

tx_power_limit

channels_to_limit_low

channels_to_limit_high

phy_mask

None

 

Arguments:

  • tx_power_limit: transmitter output power limit, expressed in dBm.
    This power limit must not be higher than the output power supported in the configured power mode.
    • Supported power modes and maximum output power levels:
      • Power mode 0: maximum 2 dBm
      • Power mode 1: maximum 6 dBm
    • channels_to_limit_low: channel selection low mask (channel 0 to channel 31); 32 bits binary mask for the channels on which the power limit is applied.

channels_to_limit_low

 

Bit position

31

30

29

28 .. 3

2

1

0

Channel #

31

30

29

28 .. 3

2

1

0

 

  • ‘0’: channel not selected
  • ‘1’: channel selected
  • Fields:
    • LSB = channel 0
    • LSB + 1 = channel 1
    • MSB = channel 31
  • channels_to_limit_high: channel selection high mask (channel 32 to channel 39); 32 bits binary mask for the channels on which the power limit is applied of which only the 8 LSBs are used

channels_to_limit_high

 

Bit position

31 ..8

7

6

5 .. 3

2

1

0

Channel #

--

39

38

37 .. 35

34

33

32

                 

 

  • ‘0’: channel not selected
  • ‘1’: channel selected
  • Fields:
    • LSB = channel 32
    • LSB + 1 = channel 33
    • LSB + 7 = channel 39
  • phy_mask: selection of PHY modes in which the output power limitation is applied; 4 bits

Bit position

3

2

1

0

PHY mode

Long Range S = 2

Long Range S = 8

2 Mbps

1 Mbps

 

  • ‘0’: PHY mode not selected
  • ‘1’: PHY mode selected
  • Fields:
    • LSB = 1 Mbps mode
    • LSB +1 = 2 Mbps mode
    • LSB +2 = Long Range S=8 mode
    • LSB +3 = Long Range S=2 mode

 

2.2      Examples

 

  • To remove the transmitter output power limit on channels 15 and 31 in both Long Range PHY modes:
    • HCI_CMD_OCF_LIMIT_PHY_TX (6, 0x00000000, 0x00000000, 0xC)
      • tx_power_limit = 6 dBm
      • channels_to_limit_low = 0x0000000, no power limit applied to any channel in range 0 .. 31
      • channels_to_limit_high = 0x00000000, no power limit applied to any channel in range 32 .. 39
      • phy_mask = 0xC = 0b1100: selection of both Long Range PHY modes

 

  • To configure a transmitter output power limit of 4 dBm on channels 15 and 31 for Long Range S=8 PHY mode:
    • HCI_CMD_OCF_LIMIT_PHY_TX (4, 0x80008000, 0x00000000, 0x4)
      • tx_power_limit = 4 dBm
      • channels_to_limit_low = 0x8008000, power limit applied to any channels 31 (MSB = 1) and 15 (MSB – 16 = 1)
      • channels_to_limit_high = 0x00000000, no power limit applied to any channel in range 32 .. 39
      • phy_mask = 0x4 = 0b0100: selection of Long Range PHY mode S=8

 

 

References: 

https://www.nxp.com/products/MCX-W23

https://www.nxp.com/docs/en/errata/ES_MCXW236XUIK.pdf

 

 

无评分
版本历史
最后更新:
‎07-09-2025 02:48 AM
更新人: