iMX8MP with IW612 (Maya-W276) configuring access point with netplan.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX8MP with IW612 (Maya-W276) configuring access point with netplan.

961件の閲覧回数
Tannerpalin
Contributor I

Hello, I am attempting to setup an access point for the iMX8MP through the Maya-W276. I am trying to configure this on uap0 with netplan and have attached my netplan .yaml configuration file. I am running a Yocto image of  NXP i.MX Release Distro 6.6-scarthgap (scarthgap). Here is my .yaml file configuration for netplan:

network:
  version: 2
  renderer: NetworkManager
  ethernets:
    eth0:
      dhcp4: true
      optional: true
  wifis:
    uap0:
      dhcp4: true
      addresses: [192.168.10.1/24]
      optional: true
      access-points:
        "test-access":
            auth:
              key-management: psk
              password: "password"
            mode: ap
            band: 2.4GHz

 

 

 

0 件の賞賛
返信
3 返答(返信)

956件の閲覧回数
Tannerpalin
Contributor I
Unfortunately I can't edit my original post, but the error seems to relate to:
wlan: uap0 Starting AP
[ 1610.613754] Get vht_cap from beacon ies: 0x33d07030
[ 1610.618653] Get vht_oprat_ie from beacon ies: chan_width=0
[ 1610.627804] wlan: uap0 AP started
[ 1610.632337] wlan: HostMlme uap0 send deauth/disassoc
[ 1610.638707] Set AC=3, txop=47 cwmin=3, cwmax=7 aifs=1
[ 1610.644641] Set AC=2, txop=94 cwmin=7, cwmax=15 aifs=1
[ 1610.650333] Set AC=0, txop=0 cwmin=15, cwmax=63 aifs=3
[ 1610.655970] Set AC=1, txop=0 cwmin=15, cwmax=1023 aifs=7
[ 1610.664586] wlan: uap0 START SCAN
o[ 1610.931158] audit: type=1325 audit(1738696175.980:48): table=nm-shared-uap0:25 family=2 entries=2 op=nft_unregister_table pid=1272 comm="nft"
[ 1610.944025] audit: type=1300 audit(1738696175.980:48): arch=c00000b7 syscall=211 success=yes exit=128 a0=3 a1=ffffd87f0c60 a2=0 a3=1 items=0 ppid=599 pid=1272 auid=4294967295 uid=0 gid)
[ 1610.970422] audit: type=1327 audit(1738696175.980:48): proctitle=2F7573722F7362696E2F6E6674002D66002D
[ 1610.992061] wlan: HostMlme uap0 send deauth/disassoc
[ 1610.997101] IOCTL failed: 000000006ffcbd71 id=0x10000, sub_id=0x10003 action=1, status_code=0x80000007
[ 1611.015914] wlan: SCAN COMPLETED: scanned AP count=14
rkManager/[ 1611.326756] wlan: uap0 Stopping AP
[ 1611.330356] wlan: uap0 AP stopped
[ 1611.335610] uap0: Skip change virtual intf type on uap: from 3 to 2
[ 1611.383227] wlan: uap0 START SCAN
0 件の賞賛
返信

921件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Is there any specific reason why you are not using hostapd?

Could you please try hostapd and tell me if it still fails? You can refer to UM11490 section 2.2.

 

Regards,

Daniel.

0 件の賞賛
返信

848件の閲覧回数
Tannerpalin
Contributor I
That's a good point, I have some success with hostapd so far and will continue down that path. I will update this after another attempt is made with hostapd.

It would be great if netplan would work so as to condense the change of network configurations to a single .yaml file.
0 件の賞賛
返信