W8997 bluetooth hciattach command timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

W8997 bluetooth hciattach command timeout

5,931件の閲覧回数
Letu
Contributor I

Hello

I attempted to use the Bluetooth functionality of W8997.

In the Yocto compiled image system, I was able to successfully load and use it using the command 'hciattach ttymxc0 any 115200 flow'. However, in the Debian system, I couldn't load it successfully

[   91.249245] Bluetooth: hci0: Frame reassembly failed (-84)
[   91.256269] Bluetooth: hci0: Frame reassembly failed (-84)
[   93.249583] Bluetooth: hci0: command 0x1003 tx timeout
[   95.265586] Bluetooth: hci0: command 0x1001 tx timeout
[   97.281586] Bluetooth: hci0: command 0x1009 tx timeout
0 件の賞賛
返信
8 返答(返信)

5,916件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Letu 

In the Yocto compiled image system, I was able to successfully load and use it using the command 'hciattach ttymxc0 any 115200 flow'.

==>Do you mean on our NXP I.MX board? Because it is using UART1 interface (/dev/ttymxc0 ) for Bluetooth.

However, in the Debian system, I couldn't load it successfully

==>So you need to check your Debian system, which UART interface is used for Bluetooth. It might be /dev/ttymxc1 or /dev/ttymxc2 or other things. So please check it.

And, may I know :

1.Your Debian system Linux kernel version? 

2.What's your host side board?

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

5,911件の閲覧回数
Letu
Contributor I

Yes, the hardware platform is i.MX 8M Plus.

The Debian system is using kernel version 5.4.70, which is actually copied from Yocto with some additional modifications.

I have tried running the Yocto Image file with the Debian file system, as well as running the Yocto file system with the Image file used by the Debian system, but I couldn't successfully load the Bluetooth functionality in both cases.

0 件の賞賛
返信

5,888件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Letu 

Can you please explain in details how to load successfully before?

Can you please check the UART interface you are using?

Please also let me know details that you build and load. Actually, I don't totally understand your repro steps.

Besides, you can power off and plug the power supply put, then plug in again then power on to have a try.

 

Best regards,

Christine.

タグ(1)
0 件の賞賛
返信

5,879件の閲覧回数
Letu
Contributor I

Hello, @Christine_Li 

 

hciattach ttymxc0 any 115200 flow
hciconfig hci0 up
hciconfig

 

After running the commands above, i should see this:

 

hci0:   Type: Primary  Bus: UART
        BD Address: 00:E9:3A:0D:D2:10  ACL MTU: 1016:5  SCO MTU: 60:12
        UP RUNNING PSCAN
        RX bytes:1415 acl:0 sco:0 events:81 errors:0
        TX bytes:1215 acl:0 sco:0 commands:81 errors:0

 

 

0 件の賞賛
返信

5,831件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Letu 

Yes, you are right, with above command, you should see the correct Bluetooth MAC address.

But, I want to know how do you boot up your I.MX8MP with Debian system in details including how did you compile the Debian system.

And as mentioned before, please check the correct Bluetooth UART interface. It might be another ttymxc... interface, different with Yocto.

 

Best regards,

Christine.

0 件の賞賛
返信

5,808件の閲覧回数
Letu
Contributor I

Thank you for your response. I have successfully resolved the issue.

The specific reason was that my Bluetooth serial port was using DMA mode, but my Debian system did not have the corresponding SDMA firmware file, which prevented DMA communication from functioning properly. When I attempted to switch the UART to interrupt mode, it started working correctly. Therefore, I identified the lack of SDMA firmware as the root cause.

0 件の賞賛
返信

5,799件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Letu 

Please forgive my lack of knowledge, would you mind to share how to check whether is working in DMA mode or interrupt mode and how to switch the UART to interrupt mode?

Appreciated if you can share for our reference.

 

Thanks and Regards,

Christine.

0 件の賞賛
返信

5,803件の閲覧回数
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @Letu 

Thanks for sharing your experience and solution to us.

It has great reference value for our future support to other customers who also use Debian system.

Appreciate it so much.

Have a nice day and weekend.

Best regards,

Christine.

0 件の賞賛
返信