8997 WiFi Crash Issue while using AP mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8997 WiFi Crash Issue while using AP mode

3,762件の閲覧回数
pratikpanchal
Contributor II

Hello NXP Team, @igorpadykov 

We are using the “Murata LBEE5XV1YM” module which is based on the “NXP 88W8997” chipset.

We are facing the attached crash while using AP mode. Request you to please guide us to get rid of the same.

Setup Details:

  • Processor:  iMX6DL processor
  • Linux Kernel Version:  4.1.15 
  • Wi-Fi Chipset: NXP 99W8997
  • Wi-Fi Linux Kernel Driver Link: Kindly check this thread.
  • Initial crash logs (Below Table): Please refer the attahced logs for more details.

mmc1: Timeout waiting for hardware interrupt. retries left=0 opcode=0

host_to_card, write iomem (1) failed: -1

write CFG reg failed

watchdog watchdog0: watchdog did not stop!

Timeout cmd id (147.120063) = 0xce, act = 0x3400

ce 00 16 00 61 10 00 00 00 34 e9 11 62 ef cd 01 

BSS type = 1 BSS role= 1

------------Dump info-----------

Commmand Timeout

mlan_processing =1

main_lock_flag =0

 

Here is the schematic snapshot.

InterfaceInterfaceRFRFPowerPower

タグ(3)
0 件の賞賛
返信
3 返答(返信)

3,643件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

You can check in the product page of the part , you will need to sign into your account and verify in the secure files, please let me know if you do not see the file so I can try to request you access to it.

 

Regards

 

 

0 件の賞賛
返信

3,651件の閲覧回数
pratikpanchal
Contributor II

Hello Estephania,

Kindly give us this FP92 release download link.

Regards,
Pratik Panchal

0 件の賞賛
返信

3,661件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

As this ticket has been discussed internally , this is just to add the information as reference

As you might know, we have 2 kind of driver releases:

  • Specific FP68 (Feature Pack 68) releases like the one you were using
  • MGPL driver : Generic FP92 releases, which include less features, but still fit to many customer needs.

 

Could you please try compiling the driver ?

 

Regards,

0 件の賞賛
返信