negative co-ordinates on tile layer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

negative co-ordinates on tile layer

9,977 次查看
manoje_s_
Contributor III

negative co-ordinates on tile layer CTRLDESCL2.POSY is resulting in corrupted rendering on the TFT.

BPP = 2bpp

Complete layer setting dump

_______address|________0________4________8________C

AZNC:40059180|>017A0320 0FFF0000 800BA6E0 4FF10011

AZNC:40059190| 00000000 00000000 00010001 00000000

AZNC:400591A0| 00000000 ???????? ???????? ????????

AZNC:400591B0| ???????? ???????? ???????? ????????

标签 (3)
0 项奖励
回复
9 回复数

9,700 次查看
juangutierrez
NXP Employee
NXP Employee

I notice that you are not enabling the layer (EN bit field = 0)

DCUx_CTRLDESCLn_4 = 0x4FF10011

EN = 0

TILE_EN = 0

DATA_SEL = 0

SAFE_EN = 0

TRANS = FF

BPP = 1 = 2bpp

RLE = 0

LU-OFFset = 1

BB = 0

AB = 1

If the layer is not even enabled maybe the source of corruption is other and not this layer.

Are you able to see the image properly displayed when POSY = 0?

Could you try using layer 64 instead of 62?

9,681 次查看
manoje_s_
Contributor III

The layer was indeed enabled when the issue was observed, I was trying various values to see when the issue happens and may be while I took the memory dump it was disabled.

The layer display properly when POSY = 0, I have verified this. Layer 64 is also tried and the issue is present there as well. I donot observe the issue with non tile layers, I tried negative co-ordinates with a RGB565 raster image layer, it was OK.

Regards,

Manoj E S

http://www.visteon.com/products/electronics/index.html

0 项奖励
回复

9,681 次查看
juangutierrez
NXP Employee
NXP Employee

I tried quickly with similar parameters in my environment and I don't see the error, however, I don't have a 2bpp image, so I tried with this format but obviously the image displayed was just blur lines. Can you share the 2bpp image source you are using and the LUT, so I can try at my side?

0 项奖励
回复

9,681 次查看
manoje_s_
Contributor III

It is just a 32bit value such as below to create a 16x1 2bpp tile image.

UINT32 tile_image = 0x00000000;

Did you see any difference when you change the Y position to -1 and 0? I am attaching screen shots showing the issue behavior.

0 项奖励
回复

9,681 次查看
juangutierrez
NXP Employee
NXP Employee

Hi Manoj

I was able to reproduce the image corruption. (I was not setting TILE_EN in my previous test). Actually it happens for other formats too (not only 2bpp).

I contacted Design team and they replied to me that this feature (negative Ypos in TileMode) by design is not implemented in Hardware.

It was decided that it should be implemented by the application via software. Only Tile layer XPOS in negative direction is supported by Hardware.

It is a mistake that this is not mentioned in RM.

This will be corrected in following Vybrid RM revisions.

So, in your application you need to take care of this, checking the YPOS in a TileLayer, if the value is negative then reduce the Vertical Layer size.

9,681 次查看
juangutierrez
NXP Employee
NXP Employee

Also, Would you post the PARR_ERR_STATUS1, PARR_ERR_STATUS2, PARR_ERR_STATUS3 registers, please?

Maybe the errors flags (if any) can give us some clues.

Other question is, what happened if you increase the tile size (specially the vertical size), does it help?

0 项奖励
回复

9,681 次查看
manoje_s_
Contributor III

These register have the value 1,0,0 respectively. There is no change when I change the POSY=-1, value remains at 1,0,0

0 项奖励
回复

9,681 次查看
naoumgitnik
Senior Contributor V

Hello Manoj,

Too "telegraph" style :smileyhappy:...

May you provide more details, please? E.g.:

  • what board are you using - yours or ours?
  • what code are you using - yours homemade or based on ours?
  • etc.

Sincerely, Naoum Gitnik.

0 项奖励
回复

9,681 次查看
manoje_s_
Contributor III

I am using FARADAY EVB from Freescale. The code used is our own code.

This is what is printed on the device

PVF522R3K1CMK4

TEST REV C2

IN02G

P62942 01

XAA1302K

Regards,

Manoj E S

0 项奖励
回复