chip configuration information: Where is it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

chip configuration information: Where is it?

Jump to solution
5,694 Views
markwatson
Contributor III

IN the Reference Manual there are several places with statements like this:

RXFIFOSIZE field: The reset value depends on whether the specific UART instance supports the FIFO and on the size of

that FIFO. See the Chip Configuration details for more information on the FIFO size supported for each

UART instance.

Where is this information?  I have looked in the Data Sheet, Reference Manual and the Fact sheet.  In several places one can find the number of UARTS, but not the really specific information such as FIFO sizes.

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
5,200 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
5,201 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
5,202 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Mark,

it is in Chapter 3: Chip Configuration.

Each IP (UART, SPI, DMA, ....) can support different configuration and it depends on the SoC design how it is configured. This chapter include those details.

/Jiri