about M4Core reboots.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about M4Core reboots.

Jump to solution
1,873 Views
soichiyamamoto
Contributor V

Hi,

I check the method that only M4Core reboots.

It is a question about CCM_CCOWR[AUX_CORE_WKUP].

Q1)

What kind of sequence do you do when you set CCM_CCOWR[AUX_CORE_WKUP]=1?

Can only secondary Core (M4Core) reboot?

Q2)

Please tell me the method that only M4Core reboots.

Best regards,

soichi

Labels (1)
0 Kudos
Reply
1 Solution
1,724 Views
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

From our understanding, there is no way to reset the M4 core without also resetting the A5 core, so there is not a method in which only the M4 core reboots.

Thanks,

Timesys Support

View solution in original post

0 Kudos
Reply
3 Replies
1,724 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 Kudos
Reply
1,725 Views
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

From our understanding, there is no way to reset the M4 core without also resetting the A5 core, so there is not a method in which only the M4 core reboots.

Thanks,

Timesys Support

0 Kudos
Reply
1,724 Views
soichiyamamoto
Contributor V

Hello

Thank you.

Best regards,

soichi

0 Kudos
Reply