about M4Core reboots.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about M4Core reboots.

ソリューションへジャンプ
1,909件の閲覧回数
soichiyamamoto
Contributor V

Hi,

I check the method that only M4Core reboots.

It is a question about CCM_CCOWR[AUX_CORE_WKUP].

Q1)

What kind of sequence do you do when you set CCM_CCOWR[AUX_CORE_WKUP]=1?

Can only secondary Core (M4Core) reboot?

Q2)

Please tell me the method that only M4Core reboots.

Best regards,

soichi

ラベル(1)
0 件の賞賛
返信
1 解決策
1,760件の閲覧回数
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

From our understanding, there is no way to reset the M4 core without also resetting the A5 core, so there is not a method in which only the M4 core reboots.

Thanks,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,760件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help on this case?

0 件の賞賛
返信
1,761件の閲覧回数
timesyssupport
Senior Contributor II

Hello Yamamoto-san,

From our understanding, there is no way to reset the M4 core without also resetting the A5 core, so there is not a method in which only the M4 core reboots.

Thanks,

Timesys Support

0 件の賞賛
返信
1,760件の閲覧回数
soichiyamamoto
Contributor V

Hello

Thank you.

Best regards,

soichi

0 件の賞賛
返信