Yocto project support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto project support

Jump to solution
7,062 Views
kubiznak_petr
Contributor V

When is there gonna be a Yocto project support for Vybrid, as it is already in progress for i.MX? Any details are appreciated. Thanks.

Labels (2)
Tags (3)
0 Kudos
Reply
1 Solution
5,046 Views
timesyssupport
Senior Contributor II

Hello Petr,

Sure. Here is a link to the sources for the meta-fsl-arm layer:

https://github.com/Freescale/meta-fsl-arm

And a link to the meta-fsl-arm-extra layer:

https://github.com/Freescale/meta-fsl-arm-extra

Finally, here is a link to the Yocto Project Quick Start guide, which has instructions to get you up and running with an initial build:

http://www.yoctoproject.org/docs/current/yocto-project-qs/yocto-project-qs.html

Thanks,

Timesys Support

View solution in original post

0 Kudos
Reply
10 Replies
5,046 Views
anindyagayen
Contributor I

As mentioned above I inserted two layers as meta-fsl-arm & meta-fsl-arm-extra. There yocto building is done successfully but at booting time it is giving System halted massage after kernel boot. Please get the total kernel logs below.

Board using: phycore vybrid (pcl052)

Host side command used for building:

          source ./oe-init-build-env

          git clone https://github.com/Freescale/meta-fsl-arm-extra.git -b dizzy

          git clone https://github.com/Freescale/meta-fsl-arm.git -b dizzy

Edited local.conf with MACHINE ??= "pcl052" and bblayers.conf and that is looking like below.

-----------------------------------------------------------------------------------------------------------------------------

# LAYER_CONF_VERSION is increased each time build/conf/bblayers.conf

# changes incompatibly

LCONF_VERSION = "6"

BBPATH = "${TOPDIR}"

BBFILES ?= ""

BBLAYERS ?= " \

  /home/user/I4_Work/poky/meta \

  /home/user/I4_Work/poky/meta-yocto \

  /home/user/I4_Work/poky/meta-yocto-bsp \

  /home/user/I4_Work/poky/meta-fsl-arm-extra \

  /home/user/I4_Work/poky/meta-fsl-arm \

  /home/user/I4_Work/poky/meta-fsl-demos \

  "

BBLAYERS_NON_REMOVABLE ?= " \

  /home/user/I4_Work/poky/meta \

  /home/user/I4_Work/poky/meta-yocto \

  "

------------------------------------------------------------------------------------------------------------------------------

          bitbake -u goggle core-image-minimal

After building successfully got the tar ball of RFS. Copied to SD card. Extracted it. Executed "sudo ln -s sbin/init ." & "sudo chown root ."

U-Boot 2011.12 (Jul 18 2016 - 14:46:44)

CPU: Freescale VyBrid 600 family rev1.3 at 0 MHz

Reset cause:

Board: Cosmic for phyCORE-Vybrid

DRAM: 256 MiB

WARNING: Caches not enabled

NAND: 512 MiB

MMC: FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In: serial

Out: serial

Err: serial

Net: Link UP timeout

FEC1

Hit any key to stop autoboot: 0

reading uImage-3.0-ts-armv7l

2521804 bytes read

## Booting kernel from Legacy Image at 80010000 ...

  Image Name: Linux-3.0.15

  Image Type: ARM Linux Kernel Image (uncompressed)

  Data Size: 2521740 Bytes = 2.4 MiB

  Load Address: 80008000

  Entry Point: 80008000

  Verifying Checksum ... OK

  Loading Kernel Image ... OK

OK

Starting kernel ...

Linux version 3.0.15 (ganindya@Ani) (gcc version 4.9.3 20150529 (release) [ARM/embedded-4_9-branch revision 227977] (GNU Tools for ARM Embedded Processors) ) #1 Mon Jul 18 14:53:58 IST 2016

CPU: ARMv7 Processor [410fc051] revision 1 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: PHYTEC Cosmic Board for phyCORE-Vybrid

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024

Kernel command line: rw mem=256M console=ttymxc1,115200n8 init=/sbin/init root=/dev/mmcblk0p3 rootwait rootfstype=ext2 mtdparts=NAND:256k(spare),256k(bootloader),128k(env),4m(kernel),-(rootfs)

PID hash table entries: 1024 (order: 0, 4096 bytes)

Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)

Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)

Memory: 256MB = 256MB total

Memory: 254648k/254648k available, 7496k reserved, 0K highmem

Virtual kernel memory layout:

  vector : 0xffff0000 - 0xffff1000 ( 4 kB)

  fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)

  DMA : 0xf4600000 - 0xffe00000 ( 184 MB)

  vmalloc : 0x90800000 - 0xf2000000 (1560 MB)

  lowmem : 0x80000000 - 0x90000000 ( 256 MB)

  modules : 0x7f000000 - 0x80000000 ( 16 MB)

  .init : 0x80008000 - 0x8002f000 ( 156 kB)

  .text : 0x8002f000 - 0x804a2bc4 (4559 kB)

  .data : 0x804a4000 - 0x804d4e40 ( 196 kB)

  .bss : 0x804d4e64 - 0x805159a0 ( 259 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1

NR_IRQS:456

MVF GPIO hardware

sched_clock: 32 bits at 66MHz, resolution 15ns, wraps every 65075ms

Console: colour dummy device 80x30

Calibrating delay loop... 262.96 BogoMIPS (lpj=1314816)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A5 PMU driver, 3 counters available

NET: Registered protocol family 16

mcf_edma: Initialized successfully

hw-breakpoint: Debug register access (0xee003e17) caused undefined instruction on CPU 0

hw-breakpoint: Debug register access (0xee004e52) caused undefined instruction on CPU 0

IMX usb wakeup probe. id=1

IMX usb wakeup probe. id=0

bio: create slab at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Advanced Linux Sound Architecture Driver Version 1.0.24.

Switching to clocksource pit

NET: Registered protocol family 2

IP route cache hash table entries: 2048 (order: 1, 8192 bytes)

TCP established hash table entries: 8192 (order: 4, 65536 bytes)

TCP bind hash table entries: 8192 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 8192 bind 8192)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Static Power Management for Freescale Vybrid

PM driver module loaded

JFFS2 version 2.2. (NAND) ? 2001-2006 Red Hat, Inc.

msgmni has been set to 497

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

Console: switching to colour frame buffer device 80x30

fb0: Layer0 fb device registered successfully.

fb1: fb device registered successfully.

fb2: fb device registered successfully.

fb3: fb device registered successfully.

Serial: MVF driver

imx-uart.1: ttymxc1 at MMIO 0x40028000 (irq = 94) is a IMX

console [ttymxc1] enabled

brd: module loaded

FSL NFC MTD nand Driver 1.0

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xcc (Micron NAND 512MiB 3,3V 16-bit)

5 cmdlinepart partitions found on MTD device NAND

Creating 5 MTD partitions on "NAND":

0x000000000000-0x000000040000 : "spare"

0x000000040000-0x000000080000 : "bootloader"

0x000000080000-0x0000000a0000 : "env"

0x0000000a0000-0x0000004a0000 : "kernel"

0x0000004a0000-0x000020000000 : "rootfs"

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.1: irq 108, io base 0x400b4000

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

g_ether gadget: using random self ethernet address

g_ether gadget: using random host ethernet address

usb0: MAC ca:22:97:6f:20:5f

usb0: HOST MAC de:0e:4d:7b:3c:e9

g_ether gadget: controller 'fsl-usb2-udc' not recognized; trying CDC Ethernet (ECM)

g_ether gadget: Ethernet Gadget, version: Memorial Day 2008

g_ether gadget: g_ether ready

fsl-usb2-udc: bind to driver g_ether

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci sdhci-esdhc-imx.1: no write-protect pin available!

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.1] using ADMA

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

Waiting for root device /dev/mmcblk0p3...

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SDHC card at address aaaa

mmcblk0: mmc0:aaaa SS08G 7.40 GiB

mmcblk0: p1 p2 p3

EXT2-fs (mmcblk0p3): warning: mounting unchecked fs, running e2fsck is recommended

VFS: Mounted root (ext2 filesystem) on device 179:3.

Freeing init memory: 156K

System halted.

0 Kudos
Reply
5,046 Views
tony_f123
Contributor III

Helllo Anindya,

A few thoughts come to mind:

-Are you using dizzy branch for your other meta-layers? You will want to do this if you have not already, and rebuild

-I am unsure of your process for extracting the rootfs to the SD card. Can you try 'sudo tar -xvf /path/to/rootfs -C /path/to/SD/card/partition'? Can you also try DDing the SD card image produced by your Yocto build to your SD card?

Thanks,

Tony

0 Kudos
Reply
5,046 Views
anindya19
Contributor I

Hi Tony,

Actually previously I was building the kernel separately using poky toolchain and rootfs taken from yocto. But now I used yocto kernel which I built using yocto build system and it is working fine. I found some modifications between yocto kernel and externel kernel source which I downloaded from "ftp://ftp.phytec.com/products/PCL-052_Cosmic-Vybrid/Linux/PD13.1.0/MCC_Demo/". Though this version of kernel is working fine with buildroot, openWRT but not working with Yocto.

Any way, thanks for giving some quick suggestions.

Thanks & regards,

Anindya

0 Kudos
Reply
5,046 Views
timesyssupport
Senior Contributor II

Hello Petr,

We have added Vybrid Tower support (machine name twr-vf65gs10) to the meta-fsl-arm Yocto project layer, and the Phytec phyCORE Vybrid (pcm052), Phytec Cosmic+ Vybrid (pcl052), and Device Solutions Quartz Vybrid (quartz) to the meta-fsl-arm-extra layer. Let me know if you have any questions.

Thanks,

Timesys Support

0 Kudos
Reply
5,046 Views
kubiznak_petr
Contributor V

Hi Timesys Support,

Thank you for your reply. Can you please point me to some related sources and/or documentation?

Thanks,

Petr

0 Kudos
Reply
5,047 Views
timesyssupport
Senior Contributor II

Hello Petr,

Sure. Here is a link to the sources for the meta-fsl-arm layer:

https://github.com/Freescale/meta-fsl-arm

And a link to the meta-fsl-arm-extra layer:

https://github.com/Freescale/meta-fsl-arm-extra

Finally, here is a link to the Yocto Project Quick Start guide, which has instructions to get you up and running with an initial build:

http://www.yoctoproject.org/docs/current/yocto-project-qs/yocto-project-qs.html

Thanks,

Timesys Support

0 Kudos
Reply
5,046 Views
mpfgregory
Contributor III

I just gave this a try on my pcm052. Worked pretty much out of the box. Great work!

The only think I had to change was:

meta-fsl-arm/conf/machine/include/imx-base.inc line 121:

KERNEL_IMAGETYPE = "zImage"

to

KERNEL_IMAGETYPE ?= "zImage"

With this change I could specify KERNEL_IMAGETYPE = "uImage" in my local.conf. The pcm052 u-boot is not configured to support bootz, so I have to use uImage.

0 Kudos
Reply
5,046 Views
kubiznak_petr
Contributor V

Perfect, thank you!

0 Kudos
Reply
5,046 Views
naoumgitnik
Senior Contributor V

Hello Ragan_Dunham,

May you comment on our plans, please?

Thanks, Naoum Gitnik.

0 Kudos
Reply
5,046 Views
Ragan_Dunham
NXP Employee
NXP Employee

We have partnered with timesyssupport for Linux support on Vybrid and they will be more than happy to help you out.  We have no plans to support a community BSP for Vybrid in Yocto.

Best Regards,

Ragan

0 Kudos
Reply