Vybrid support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,640件の閲覧回数
JohnBirch
NXP Employee
NXP Employee

Do we have any support for Wifi and BlueTooth (BT or BTLE) on Vybrid?

0 件の賞賛
返信
1 解決策
1,450件の閲覧回数
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

元の投稿で解決策を見る

3 返答(返信)
1,451件の閲覧回数
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

1,450件の閲覧回数
rendy
NXP Employee
NXP Employee

Hi,

Timesys support should provide list of USB dongles supported by their kernel.

Regards

Rene

1,450件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to attend this case?

0 件の賞賛
返信