Vybrid support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid support

跳至解决方案
1,688 次查看
JohnBirch
NXP Employee
NXP Employee

Do we have any support for Wifi and BlueTooth (BT or BTLE) on Vybrid?

0 项奖励
回复
1 解答
1,498 次查看
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

在原帖中查看解决方案

3 回复数
1,499 次查看
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

1,498 次查看
rendy
NXP Employee
NXP Employee

Hi,

Timesys support should provide list of USB dongles supported by their kernel.

Regards

Rene

1,498 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to attend this case?

0 项奖励
回复