Vybrid support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid support

Jump to solution
1,703 Views
JohnBirch
NXP Employee
NXP Employee

Do we have any support for Wifi and BlueTooth (BT or BTLE) on Vybrid?

0 Kudos
Reply
1 Solution
1,513 Views
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

View solution in original post

3 Replies
1,514 Views
timesyssupport
Senior Contributor II

Hello John,

Specifically, we have validated a TiWi/BLE wl12xx based module on a custom platform; that did require kernel patches and device tree modifications, and was present on the custom board.

Devices listed at the following are provided in the 3.13, but none have been specifically validated:

Networking support > Bluetooth subsystem support > Bluetooth device drivers

Device Drivers > Network device support > USB Network Adapters

Necessary firmware/BTS would need to obtained when not provided in kernel.

Thank you,

Timesys Support

1,513 Views
rendy
NXP Employee
NXP Employee

Hi,

Timesys support should provide list of USB dongles supported by their kernel.

Regards

Rene

1,513 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you help to attend this case?

0 Kudos
Reply