Vybrid VF6xx I2S Audio Codec Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vybrid VF6xx I2S Audio Codec Connection

3,589 次查看
juandiaz
Contributor II

Hello,

I am a newbie in I2S interface for audio codec chips. I need to connect a codec WM8974 of Cirrus/Wolfson, which has a mono audio speaker and a microphone. The WM8974 has the following digital I/O pinout:

I2S Interface:

- ADCDAT (O): ADC digital audio data output

- DACDAT (I): DAC digital audio data input

- FRAME (I/O): DAC and ADC sample rate clock or frame sync

- BCLK (I/O): Digital audio port clock

- MCLK (I): Master clock input

Control Interface (2-Wire / 3-Wire):

- CSB/GPIO (I/O): 3-Wire MPU chip select or general purpose input/output pin.

- SCLK (I): 3-Wire MPU clock Input / 2-Wire MPU Clock Input

- SDIN (I/O): 3-Wire MPU data Input / 2-Wire MPU Data Input

- MODE (I): Control interface mode selection pin.

In one hand, I am going to set the Control Interface to 2-Wire (MODE=low) in order to use the Vybrid I2C interface (SCLK / SDATA). This is quite easy.

On the order hand, regarding the I2S interface, if I am going to use the codec as slave, theoretically, I will connect the Vybrid as follows:

Vybrid                            Codec

---------                           --------

SAIx_RX_DATA     <----    ADCDAT

SAIx_TX_DATA     ---->    DACDAT

SAIx_TX_BCLK      ---->    BCLK

SAIx_TX_SYNC     ---->    FRAME

If I connect the audio codec as master, the pinout connection will be:

Vybrid                            Codec

---------                           --------

SAIx_RX_DATA     <----    ADCDAT

SAIx_TX_DATA     ---->    DACDAT

SAIx_RX_BCLK      <----    BCLK

SAIx_RX_SYNC     <----    FRAME

My question is if these connections are OK for use of the SAI/I2S interfaces (SAI0, SAI1, ...) of the Vybrid VF6xx.

Kind Regards,

Juan.

标签 (1)
5 回复数

3,038 次查看
timesyssupport
Senior Contributor II

Hi Juan,
              >Can you tell me which value has tsys?
According to the WM8974 wolfson audio codec document - ESAI (enhanced serial audio interface) clock cycle(Tssicc) = 30ns.  
S12 is i2s_BCLK pulse width high (S11) and pulse width low (S11) - which is approximately 130ns.   Please refer the attached tabular column.

tab.png

Thanks,
Timesys support.

3,038 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ please continue with the follow up.

0 项奖励
回复

3,038 次查看
fernandoalcaide
Contributor II

Dear,

In Document Number VYBRIDFSERIESEC appears S11 is 4*tsys. Can you tell me which value has tsys"?

pastedImage_1.png

Thank you in advance.

0 项奖励
回复

3,038 次查看
timesyssupport
Senior Contributor II

Hi Juan,

               Selection between the two wire and 3 wire can be done using Mode bit. If MS=1 3-wire mode is selected and viceversa.

In the master mode (MS bit set to 1), clock signals BCLK, and FRAME can be outputs when the WM8974 operates as a master and BCLK, FRAME can be inputs when the WM8974 operates as a slave (MS bit set to 0) as you given.

As per the WM8974 audio codec document the above given configuration should work.

Thanks,

Timesys support.

3,038 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport​ can you take this case?

0 项奖励
回复