Vybrid VF610 instability at 500Mhz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vybrid VF610 instability at 500Mhz

1,482 次查看
HeMyFAE
NXP Employee
NXP Employee

We are looking at running our VF610s at 500 MHz and are running into some issues.  The custome have applied the 5))MHz patches that are ontop of u-boot 2013.07, provided by Timesys, against u-boot 2015.07 and see instability after 5 hours. Is there a patchset from NXP that also handle e6235 ( ANADIG: Unstable clock if PFD_FRAC divisor is 19)?

Is Timesys Uboot the latest to support 500Mhz or do we have more updated one?

Regards,

hy

标签 (1)
0 项奖励
回复
1 回复

1,291 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid we do not provide Linux BSP for Vybrid, assuming third party (Timesys) for it.

Regards,

Yuri.

0 项奖励
回复