Vybrid Unique Identifier

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid Unique Identifier

2,222 Views
kubiznak_petr
Contributor V

Hello,

where in Vybrid registers is stored a unique MCU identifier, like SIM_UIDx on Kinetis?

Labels (1)
0 Kudos
Reply
3 Replies

1,907 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Petr,

you can use OTP memory space (see following table from RM) together with other identifiers from OTP memory MSCM module ( MSCM_CPxTYPE and others )

pastedImage_2.png

to program fuses use Vybrid Sample Code.

/Jiri

1,907 Views
jiri-b36968
NXP Employee
NXP Employee

Hello Petr,

general purpose customer defined information field also can be used.

But have to correct previous reply (better later then never): Vybrid 64 bit Unique ID is located in OTP Bank 0 word 1 and 2. More in Security reference manual.

/Jiri

1,907 Views
kubiznak_petr
Contributor V

Hi Jiri,

Thank you, that helps.

Petr

0 Kudos
Reply