Vybrid Unique Identifier

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid Unique Identifier

2,180件の閲覧回数
kubiznak_petr
Contributor V

Hello,

where in Vybrid registers is stored a unique MCU identifier, like SIM_UIDx on Kinetis?

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

1,865件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hello Petr,

you can use OTP memory space (see following table from RM) together with other identifiers from OTP memory MSCM module ( MSCM_CPxTYPE and others )

pastedImage_2.png

to program fuses use Vybrid Sample Code.

/Jiri

1,865件の閲覧回数
jiri-b36968
NXP Employee
NXP Employee

Hello Petr,

general purpose customer defined information field also can be used.

But have to correct previous reply (better later then never): Vybrid 64 bit Unique ID is located in OTP Bank 0 word 1 and 2. More in Security reference manual.

/Jiri

1,865件の閲覧回数
kubiznak_petr
Contributor V

Hi Jiri,

Thank you, that helps.

Petr

0 件の賞賛
返信