Vybrid RTC reset after power off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybrid RTC reset after power off

Jump to solution
3,427 Views
jeremyesquirol
Contributor III

Hi Vybrid's users.

I'm having trouble with the SNVS RTC on Phycore Vybrid board using linux. We have the last revision of Vybrid : "2N02G" (with the VBAT issue solved) and it seems that time is lost when we powered off the board, while we have a battery (Vbat = 3.1V).

We used the default SNVS_RTC driver and looking the source file,  it's said that snvs-rtc is used in non secure mode, is that why the time is not stored? it's a normal feature?

0 Kudos
Reply
1 Solution
2,718 Views
jeremyesquirol
Contributor III

Hi Naoum and Timesys support.

We've found an issue... On their new SoM revision Phytec dont tied the coin cell to the VBAT. They use a jumper placed on the SoM that don't appears on our schematics (J8 on new schematics). The jumper is not set by default, just add a 0 resistor to tied Vbat to Vbat_in (2-3 pads).

View solution in original post

0 Kudos
Reply
5 Replies
2,718 Views
naoumgitnik
Senior Contributor V

Dear Jeremy,

Please, take a look at the Re: RTC in TWR-Vybrid doesn't keep time thread - it might help.

Regards, Naoum Gitnik.

[timesyssupport]

2,718 Views
jeremyesquirol
Contributor III

Hi Naoum,

I wiil try with a lower resistance but I dont think itt will solve this problem. As I said before, I use the last revision of Vybrid, with Hardware VBAT problem solved. (when main supply is off, Vbat is 3,1V and about 3µA)

The RTC is keeping right time if the board isn't switched off. If the main supply is lost the RTC is reset to 01/01/1970, 00:00:00.

I have a 3V battery attached and the VBAT tied to Coin Cell

0 Kudos
Reply
2,719 Views
jeremyesquirol
Contributor III

Hi Naoum and Timesys support.

We've found an issue... On their new SoM revision Phytec dont tied the coin cell to the VBAT. They use a jumper placed on the SoM that don't appears on our schematics (J8 on new schematics). The jumper is not set by default, just add a 0 resistor to tied Vbat to Vbat_in (2-3 pads).

0 Kudos
Reply
2,718 Views
timesyssupport
Senior Contributor II

Hello Jérémy,


I have observed this behavior on the Vybrid Tower in the past. I will attempt to reproduce on the pcm052, and let you know what I find. If this is an issue on the pcm052, I don't have an estimated ETA for a fix. If this is a time-sensitive issue for you, I would recommend escalating with Timesys under a services agreement.

Thanks,

Timesys Support

2,718 Views
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you  help with this case?

0 Kudos
Reply