Vybrid Non Xip Qspi Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid Non Xip Qspi Boot

跳至解决方案
2,323 次查看
ngsari
Contributor II

Hello Folks;
MQX QSPI Non-Xip boot works just fine.
However I would like place some MQX librarys in the QSPI FLash. I don't want load them in to the Internal SRAM.

What should I do with Scatter file ? (MQX BSP and PSP must placed in RAM)

I tried to add some load / execution regions with base 0x20040000. Doesn't seems to work. (Or generate 512MB Image file)

Thank you for time.

#! armcc -E --cpu Cortex-A5.neon

#define CODE_BASE_ADDR_START     0x3F000000

#define CODE_BASE_ADDR_END       0x3F03FFF0

#define CODE_SIZE               (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START)

#define DATA_BASE_ADDR_START     0x3F050000

#define DATA_BASE_ADDR_END       0x3F070000

#define DATA_SIZE               (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)

#define DATA_SHARED_START       0x3F040000

#define DATA_SHARED_END         0x3F04FFF0

#define RESERVED_BASE_ADDR_START    0x3F07EBF0

#define RESERVED_BASE_ADDR_END      0x3F07EFF0

#define RESERVED_SIZE               (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START)

#define BOOT_STACK_SIZE         0x100

#define FIQ_STACK_SIZE          0

#define ABT_STACK_SIZE          0

#define UND_STACK_SIZE          0

#define SYS_STACK_SIZE          0

QUAD_SPI_CONFIG CODE_BASE_ADDR_START

{

   CONF +0 0x400

  {

 

    *(.conf)

  }

}

BOOT_IVT_HEADER_OFFSET (CODE_BASE_ADDR_START + 0x400)

{

  IVT +0  0x20

  {

  *(.ivt)

  }

  BOOT_DATA +0 0x10

  {

  *(.boot_data)

  }

  DCD +0

  {

  *(.dcd)

  }

}

LOAD_REGION_CODE (CODE_BASE_ADDR_START + 0x800)

{

    BOOT +0

    {

        *(STARTUP)

    }

   

    CODE +0

    {

        * (InRoot$$Sections)      ; All library sections for example, __main.o,

                                  ; __scatter*.o, __dc*.o, and * Region$$Table

  * (KERNEL)

        * (TEXT)

        * (+RO)

    }

    DATA DATA_BASE_ADDR_START ALIGN 32

    {

        * (+RW, +ZI)

    }

    ; FIQ stack

    FIQ_STACKS +0 ALIGN 8 EMPTY FIQ_STACK_SIZE {}

    ; ABT stack

    ABT_STACKS +0 ALIGN 8 EMPTY ABT_STACK_SIZE {}

    ; UND stack

    UND_STACKS +0 ALIGN 8 EMPTY UND_STACK_SIZE {}

    ; SYS stack

    SYS_STACKS +0 ALIGN 8 EMPTY SYS_STACK_SIZE {}

    KERNEL_DATA_START +0 ALIGN 16

    {

        * (KERNEL_DATA_START)     ; start of kernel data

        * (SRAM_POOL_START)

        * (UNCACHED_DATA_START)

    }

    KERNEL_DATA_END DATA_BASE_ADDR_END - (0x03*0x10)      ; RAM_END - 3 x aligned value with align 0x04

    {

        * (SRAM_POOL_END)

        * (UNCACHED_DATA_END)

        * (KERNEL_DATA_END)     ; end of kernel data

    }

    SHARED_RAM_START DATA_SHARED_START 0xFFF0

    {

  *(SHARED_RAM_START)

    }

    SHARED_RAM_END DATA_SHARED_END

    {

        *(SHARED_RAM_END)

    }

   

    ; mem_init writes a storeblock_struct at the end of kernel data,

    ; max size 32 bytes, so use 0x100 offset

  

    BOOT_STACK_ADDR (DATA_BASE_ADDR_END - BOOT_STACK_SIZE) OVERLAY

    {

        *(BOOT_STACK)

    }

    ; We don't use their stack or heap, but the tools expect this

    ; to be here, so we have a dummy placeholder.

    ARM_LIB_STACKHEAP (DATA_BASE_ADDR_END - 0x100) OVERLAY EMPTY UNINIT 0x04

    { }

   

   

    RESERVED RESERVED_BASE_ADDR_START ALIGN 16

    {

        * (.boot_reserved_data)

        * (.boot_reserved_code)

    }

}

标签 (7)
0 项奖励
回复
1 解答
1,928 次查看
timesyssupport
Senior Contributor II

Hello,

Have you set the BSPCFG_ENABLE_QUADSPI0 macro to '1' in your BSP config? Can you try another address in the 0x20000000-0x2fffffff range? Let me know.

Thanks,

Timesys Support

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,929 次查看
timesyssupport
Senior Contributor II

Hello,

Have you set the BSPCFG_ENABLE_QUADSPI0 macro to '1' in your BSP config? Can you try another address in the 0x20000000-0x2fffffff range? Let me know.

Thanks,

Timesys Support

0 项奖励
回复
1,928 次查看
ngsari
Contributor II

Yes I did. Because of that I have put  MQX kernel in ram.
I'm going to try. Thank you for your time.

0 项奖励
回复
1,928 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

timesyssupport can you help with this case?

0 项奖励
回复