Vybrid NAND flash repartitioning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid NAND flash repartitioning

4,136件の閲覧回数
JaclynM
Contributor I

I'm using a Phytec PCM052 board with ARM DS-5 and Timesys toolchain.
Due to an update of U-Boot I need to repartition the flash mem.


Is there a step by step guide available from NXP using the tools from Linux-Busybox ?

I've found two reserved partitions.
According to the VybridRM the start partition holds the Firmware Configuration Block (FCB) containing primary/secondary U-Boot addresses.
Which program writes the initial values into flash ?

What is the second partition at the end of the flash used for ? Bad Block Marking Table ?


ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

4,115件の閲覧回数
kef2
Senior Contributor V
  • Due to an update of U-Boot I need to repartition the flash mem.

Why? You need to "nand erase.part <u-boot-partition>" or "nand erase <offset> <size>" the same U-Boot locations and nand write there new U-boot. Why repartition? 

NAND partitioning is done defining U-Boot default mtdparts variable. You may temporarily edit this variable to repartition NAND, but in case U-Boot environment settings are lost, default mtdparts shouldn't lead to disasters on rootfs or othe partitions.

  • According to the VybridRM the start partition holds the Firmware Configuration Block (FCB) containing primary/secondary U-Boot addresses.
    Which program writes the initial values into flash ?

Toradex U-Boot had writebcb command, which was used to create BCB taking primary and optional secondary U-boot offsets in NAND and write created BCB to start of NAND. Alternatively you may create BCB file on PC, deliver somehow to U-Boot on target and nand write it. 

  • What is the second partition at the end of the flash used for ? Bad Block Marking Table ?

It is up to you or your SOM vendor. Minimally mtdparts should include 3 partitions, one reserved for BCB, one or two for U-Boot copies, one for UBI (which may include several UBI volumes) or any other kind for partition(s) for rootfs, device tree and kernel.

0 件の賞賛
返信

4,119件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You can put in second partition the rootfs or bad block marking table but remember that the flash must be completely erase before burn. NXP don;t have any document about it.

 

Regards

0 件の賞賛
返信