The following code crashes on my Vybrid M4. The code is not even executed, but mqxboot already crashes the Linux kernel when uploading the binary.
struct xxx {
int a;
int b;
};
struct xxx bla = {1, 5};
If I use struct xxx bla = {0, 0}; instead, it works fine. Using initialized variables !=0 that are not structs also work. It happens only when I initialize structs with something != 0.
I wonder in which section the initialized structs are placed. In the .map file I see only functions, not variables. I have tried using
__attribute__((section("RAM_VECTORS")))
but the crash still happens. When building I get a linker warning:
FreescaleMQXRTOS4.0.1/lib/pcm052_m4.ds5/debug/bsp/ram.scf", line 42 (column 20): Warning: L6314W: No section matches pattern vectors.o(.vectors_ram).
I guess the structs should be placed in this section, but apparently nothing is put there. Does anybody know how to set-up the scatter file so that the initialized structs are placed in the correct section?
解決済! 解決策の投稿を見る。
Hello Timesys,
Thanks for your answer. I've found the problem. The .data segment was not part of the created binary. Below is the relevant part of my scatter file. The RW and ZI were put to address 0x3f800000, the code to address 0x3f000000. The created binary was 86kB large and was written to 0x3f000000 by mqxboot. So the RW and ZI region was uninitialized. If I put RW and ZI to the CODE region, it works fine. I guess this is not a good way to handle the problem. Do you have a more proper solution?
Best regards
Michael
| #define CODE_BASE_ADDR_START | 0x3f000000 |
| #define CODE_BASE_ADDR_END | 0x3f03fff0 |
| #define CODE_SIZE | (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START) |
| #define DATA_BASE_ADDR_START | 0x3f800000 |
| #define DATA_BASE_ADDR_END | 0x3f807ff0 |
| #define DATA_SIZE | (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START) |
| #define DATA_SHARED_START | 0x3f040000 |
| #define DATA_SHARED_END | 0x3f04fff0 |
| #define TCML_END | 0x1f807ff0 |
;
; Note:
; memory range 0x3f07ebf0 - 0x3f07eff0 is reserved for bootloader_vybrid segment
;
#define MY_ALIGN(address, alignment) ((address + (alignment-1)) AND ~(alignment-1))
LOAD_REGION_INTRAM CODE_BASE_ADDR_START
{
| VECTORS CODE_BASE_ADDR_START | ||
| { | ||
| vectors.o (.vectors_rom,+FIRST) | ||
| vectors.o (.cfmconfig) | ||
| } | ||
| CODE +0 | ||
| { | ||
| * (InRoot$$Sections) | ; All library sections for example, __main.o, | |
| ; __scatter*.o, __dc*.o, and * Region$$Table | ||
| * (KERNEL) | ||
| * (TEXT) | ||
| * (+RO) | ||
| } | ||
| RAM_VECTORS DATA_BASE_ADDR_START ; For ram vector table. Used when MQX_ROM_VECTORS is set to zero. | ||
| { | ||
| vectors.o (.vectors_ram) | ||
| } | ||
| DATA +0 ALIGN 32 | ||
| { | ||
| * (+RW, +ZI) | ||
| } |
Hello Mpfgregory,
Thanx for letting us know.
Have a great day,
Victor
Hi Mpfgregory,
In the below link you may find useful information for editing the scatter file.
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN5127.pdf
And in the below link a similar problem has been addressed by ARM,
If you still faced any issue can you please share your scatter file, so that we can have look at it and check for any errors.
Thanks,
Timesys support Engineer.
Hello Timesys,
Thanks for your answer. I've found the problem. The .data segment was not part of the created binary. Below is the relevant part of my scatter file. The RW and ZI were put to address 0x3f800000, the code to address 0x3f000000. The created binary was 86kB large and was written to 0x3f000000 by mqxboot. So the RW and ZI region was uninitialized. If I put RW and ZI to the CODE region, it works fine. I guess this is not a good way to handle the problem. Do you have a more proper solution?
Best regards
Michael
| #define CODE_BASE_ADDR_START | 0x3f000000 |
| #define CODE_BASE_ADDR_END | 0x3f03fff0 |
| #define CODE_SIZE | (CODE_BASE_ADDR_END - CODE_BASE_ADDR_START) |
| #define DATA_BASE_ADDR_START | 0x3f800000 |
| #define DATA_BASE_ADDR_END | 0x3f807ff0 |
| #define DATA_SIZE | (DATA_BASE_ADDR_END - DATA_BASE_ADDR_START) |
| #define DATA_SHARED_START | 0x3f040000 |
| #define DATA_SHARED_END | 0x3f04fff0 |
| #define TCML_END | 0x1f807ff0 |
;
; Note:
; memory range 0x3f07ebf0 - 0x3f07eff0 is reserved for bootloader_vybrid segment
;
#define MY_ALIGN(address, alignment) ((address + (alignment-1)) AND ~(alignment-1))
LOAD_REGION_INTRAM CODE_BASE_ADDR_START
{
| VECTORS CODE_BASE_ADDR_START | ||
| { | ||
| vectors.o (.vectors_rom,+FIRST) | ||
| vectors.o (.cfmconfig) | ||
| } | ||
| CODE +0 | ||
| { | ||
| * (InRoot$$Sections) | ; All library sections for example, __main.o, | |
| ; __scatter*.o, __dc*.o, and * Region$$Table | ||
| * (KERNEL) | ||
| * (TEXT) | ||
| * (+RO) | ||
| } | ||
| RAM_VECTORS DATA_BASE_ADDR_START ; For ram vector table. Used when MQX_ROM_VECTORS is set to zero. | ||
| { | ||
| vectors.o (.vectors_ram) | ||
| } | ||
| DATA +0 ALIGN 32 | ||
| { | ||
| * (+RW, +ZI) | ||
| } |
timesyssupport can you help here?