Vybrid IOMUX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid IOMUX

跳至解决方案
1,120 次查看
rkd
Contributor I

Hi,

is there any IOMUX tool for the vybrid series?

Could you also confirm if the following mapping is correct?

UART0:

- SCI0-TX, RX, CTS, RTS

UART1:

- SCI1-TX, RX, CTS, RTS

UART2:

- SCI2-TX, RX, CTS, RTS

UART3:

- SCI3-TX, RX, CTS, RTS


UART4:

- SCI4-TX, RX, CTS, RTS

I found all of the above on ball pin mapping.

But, 19.8.2.2 of the reference manual is telling me differently? 

Thanks

~RD

0 项奖励
回复
1 解答
784 次查看
MehmetAliIpin
Contributor V

Dear R D,

if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...

you will se two  excel tables on the upper left hand corner of the pdf file. These  are the IOMUX tools forr Vybrid series.

Mehmet Ali

在原帖中查看解决方案

0 项奖励
回复
1 回复
785 次查看
MehmetAliIpin
Contributor V

Dear R D,

if you dpwnload the reference manual from http://cache.freescale.com/files/32bit/doc/ref_manual/VYBRIDRM.pdf?fpsp=1&WT_TYPE=Reference%20Manual...

you will se two  excel tables on the upper left hand corner of the pdf file. These  are the IOMUX tools forr Vybrid series.

Mehmet Ali

0 项奖励
回复