Vybrid CPU frequency modification commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid CPU frequency modification commands

ソリューションへジャンプ
1,755件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

Are there any Linux commands for changing the CPU frequency on Vybrid?

i.MX has a set of echo commands, do we have anything similar to that with Vybrid?

If not, what's the best way to change the CPU frequency on the fly?

ラベル(3)
0 件の賞賛
返信
1 解決策
1,410件の閲覧回数
timesyssupport
Senior Contributor II

Hello Juan,

In the Timesys 3.0 Linux kernel for Vybrid, there is no way to change the frequency on the fly. You will need to modify kernel source to do so. Kernel 3.10+ will have better support for clocking, so on-the-fly frequency change may be a possilbility.

Thanks,

Timesys Support

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,410件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

So, is there any other way to modify on the fly the frequencies? or this is only possible modifying directly on the kernel with something like:

clk = clk_get(NULL, "pll1_main_clk");

clk_set_rate(clk, rate);

0 件の賞賛
返信
1,411件の閲覧回数
timesyssupport
Senior Contributor II

Hello Juan,

In the Timesys 3.0 Linux kernel for Vybrid, there is no way to change the frequency on the fly. You will need to modify kernel source to do so. Kernel 3.10+ will have better support for clocking, so on-the-fly frequency change may be a possilbility.

Thanks,

Timesys Support

0 件の賞賛
返信
1,410件の閲覧回数
timesyssupport
Senior Contributor II

Hello Juan,

In the current Linux BSP for Vybrid, there are no userspace commands for changing the CPU frequency.

We have had several inquiries about this, and will be reviewing this as a possibility as we update the supported Vybrid kernel to 3.10 or newer, planned for end of Q1. I will let you know when I have more information available.

Thanks,

Timesys Support

1,410件の閲覧回数
juangutierrez
NXP Employee
NXP Employee

timesyssupport can help on this, please?

0 件の賞賛
返信