Vybrid Boot pin setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Vybrid Boot pin setting

跳至解决方案
4,833 次查看
AhmedShameemM_H
Contributor I

Dear Sir,


In Freescale Tower system module, there is buffer used for isolation (see attachment) on Vybrid Boot setting pins.But for other Freescale processor’s reference boards like i.MX53 QSB, i.MX6 SDB etc. usually resistor isolation only provided.Buffer is must or Is there any specific reason for using this buffer in Vybrid reference board?

Waiting for your valuable feedback.

Thank You, in advance.

Regards,

Shameem

标签 (2)
0 项奖励
回复
1 解答
4,528 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Shameem,

  See this thread for an explanation for the buffers: Re: Vybrid GPIO Boot override

-Anthony

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,529 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Shameem,

  See this thread for an explanation for the buffers: Re: Vybrid GPIO Boot override

-Anthony

0 项奖励
回复
4,528 次查看
AhmedShameemM_H
Contributor I

Thank you , Anthony

0 项奖励
回复